===================================================================================
   			Lens Driver Controller Release Notes
===================================================================================

Release Notes: 1.10 (133898-00-A)
-------------------------------------

[Added Features]
 Updated driver installation help
 Added firmaware Type F compatibility

[Resolved Bugs]
 None

[Known Limitations]
 None

[Reqiured User Actions]
 None

[Compatibility]
 Compatibility firmware
   - 1.8.X (133899-00-A)
   - 1.9.X (133899-00-A)
   - 1.9.X (133899-00-F)
 Incompatible firmware
   - 1.3.X (133899-00-A)
   - 1.7.X (133899-00-A)


Release Notes: 1.9.5933 (133898-00-A)
-------------------------------------

[Added Features]
 Updated driver installation help

[Resolved Bugs]
 None

[Known Limitations]
 None

[Required User Actions]
 None

[Compatibility]
 Compatibility firmware
  - Type A - 1.8.X / 1.9.X
  - Type F - 1.0.X
 Incompatible firmware
  - Type A - 1.3.X / 1.7.X

Release Notes: 1.9.5765 (133898-00-A)
-------------------------------------

[Added Features]
 Lens Driver Controller compatible to type F firmware 1.0.X

[Resolved Bugs]
 Software does not crash when uEye framework is not installed and the user tries to open uEye viewer

[Known Limitations]
 None

[Required User Actions]
 None

[Compatibility]
 Compatibility firmware
  - Type A - 1.8.X / 1.9.X
  - Type F - 1.0.X
 Incompatible firmware
  - Type A - 1.3.X / 1.7.X


Release Notes 1.9.5722 (133898-00-A)
------------------------------------

[Added Features]
 Framework extended to be compatible with upcoming firmware type releases
 Signed Lens Driver driver included in the package
 Ability to detect wether a connected Lens is compatible with the Lens Driver firmware
 User is notified if outdated firmware on Lens Driver is detected
 Incorporated "Expert Mode" into general user interface
 Incorporated updated/new commands (see Lens Driver communication protocol definition)

[Resolved Bugs]
 Software does not crash when uEye framework is not installed and the user tries to open uEye viewer

[Known Limitations]
 None

[Required User Actions]
 None

[Compatibility]
 Compatible Firmware: 
  - Lens Driver V4 Firmware 1.8.X
  - Lens Driver V4 Firmware 1.9.X
 Incompatible Firmware: 
  - Lens Driver V4 Firmware 1.3.X
  - Lens Driver V4 Firmware 1.7.X



Release Notes 1.8.5308.XXXXX
----------------------------

[Features]
Backwards compatibility with Lens Driver firmware version 1.7.1147.XXXXX

[Fixed Bugs]
uEye Camera Viewer notification panel fix.
Serial ID error message bug fix.

[Known Limitations]
Only fully tested for the EL-10-30-C  and El-6-18 lens 

[Compatibility]
 Compatible Firmware: 
  - Lens Driver V4 Firmware 1.8.1230.XXXXX and up
 Working Firmware: 
  - Lens Driver V4 Firmware 1.7.1149.XXXXX



Release Notes 1.8.5281.XXXXX
--------------------

[Features]
 El-6-18 lens support
 Firmware Analog mode is now available

[Fixed Bugs]
 Sensor control mode only works after opening the lookup table window and closing it again.

[Known Limitations]
 Only fully tested for the EL-10-30-C  and El-6-18 lens 

[Compatibility]
 Compatible Firmware: 
  - Lens Driver V4 Firmware 1.8.1230.XXXXX and up



Release Notes 1.8.5199.XXXXX
--------------------

[Features]
 Focal power sensor control has been re-enabled and improved.
 DC mode sensor control has been implemented.
 Creep compensation drift gain variable has been implemented with an accuracy of 0.01.
 Improved error message readability.
 Improved backwards compatibility (1.5 and up).
 Toolstrip icon for enabled sensor control included.
 Analop input "View" option included.
 Updated software with the latest OptotuneComponent.
 Rectangular, Sinusoidsal, and Triangular sessions are restored.

[Bug Fixes]
 Analog input read fixed with latest firmware version.
 Max current is now restricted to 0-655 mA in expert mode.
 Focal power mode is now hidden if a lens with an empty/invalid EEPROM structure is connected.

[Known Limitations]
 Only fully tested for the EL-10-30-C lens 

[Compatibility]
 Compatible Firmware: 
  - Lens Driver V4 Firmware 1.7.1147.XXXXX and up
 Outdated Firmware:
  - Lens Driver V4 Firmware 1.6.0.0 
  - Lens Driver V4 Firmware 1.5.0.0
 Incompatible Firmware: 
  - Lens Driver V4 Firmware 1.3.0.0



Release Notes 1.8.5196.XXXXX
--------------------

[Features]
 Bug Fixes from 1.8.5192.XXXXX

[Bug Fixes]
 Deleting of rows in Sensor Control Configuration Form is more stable
 Sensor Control Configuration Form does not constantly ask to save table when autofocusing in ueye viewer
 Fixed interpolation error where only the first two calibration points were being used
 Fixed error where it was needed to select "Sensor Control" twice

[Known Limitations]
 Only fully tested for the EL-10-30-C lens 

[Compatibility]
 Compatible Firmware: 
  - Lens Driver V4 Firmware 1.7.1140.57667 and up
 Outdated Firmware:
  - Lens Driver V4 Firmware 1.6.0.0 
  - Lens Driver V4 Firmware 1.5.0.0
 Incompatible Firmware: 
  - Lens Driver V4 Firmware 1.3.0.0



Release Notes 1.8.5192.XXXXX
--------------------

[Features]
 Focal power sensor control has been re-enabled and improved.
 DC mode sensor control has been implemented.
 Creep compensation drift gain variable has been implemented with an accuracy of 0.01.
 Improved error message readability.
 Improved backwards compatibility (1.5 and up).
 Toolstrip icon for enabled sensor control included.
 Analop input "View" option included.
 Updated software with the latest OptotuneComponent.
 Rectangular, Sinusoidsal, and Triangular sessions are restored.

[Bug Fixes]
 Analog input read fixed with latest firmware version.
 Max current is now restricted to 0-655 mA in expert mode.
 Focal power mode is now hidden if a lens with an empty/invalid EEPROM structure is connected.

[Known Limitations]
 Only fully tested for the EL-10-30-C lens 

[Compatibility]
 Compatible Firmware: 
  - Lens Driver V4 Firmware 1.7.1140.57667 and up
 Outdated Firmware:
  - Lens Driver V4 Firmware 1.6.0.0 
  - Lens Driver V4 Firmware 1.5.0.0
 Incompatible Firmware: 
  - Lens Driver V4 Firmware 1.3.0.0